12/15/2017 3:34 PM | |
Joined: 10/5/2016 Last visit: 12/13/2022 Posts: 82 Rating: (46) |
Hello, there is an application example availible as well: https://support.industry.siemens.com/cs/ww/de/view/38132261 This might help you. Kind regards Marco |
This contribution was helpful to1 thankful Users |
12/22/2017 6:02 AM | |
Joined: 7/5/2016 Last visit: 10/9/2023 Posts: 48 Rating: (0) |
Hello bg2492 , meisterlampe34 and everybody After I open WinCC Connectivity sample project and open some document such as wincc/wincc connectivity pack V7.3 , I use OLE DB provider to query from SQL Server. I think , the manual in that link which I attach , I should see in page 219 and next. I create VBS in global script for sub SplitDateTimeMs and another sub , I change private sub command_click to sub command click. And change Dim variable As value to Dim variable only. When I compile , everything is ok. But when I activated project , my project has error about this script. Where is the wrong point such as global script writing , syntax or something inside the code? I do follow OpConPack from WinCC Disc , it's nice when open project. If I need to use follow that , It's not work because I don't know where is the SplitDateTimeMs function. After this , I will try follow meisterlampe34 ' link again. Best Regard Adam |
Last edited by: Jen_Moderator at: 12/22/2017 11:06:43 AMInserted right link. |
|