3/25/2022 4:24 PM | |
Joined: 5/30/2014 Last visit: 4/25/2025 Posts: 170 Rating:
|
It is completely ridiculous that Pro version does not support switches! I have made a bunch of basic panels screens with graphics and now I do not have adequate solution on WinCC SCADA (very expensively paid!)!! HugoD solution is very good and almost perfect. Only problem is that Button object is not connected to the tag which should be affected, only via events. In practice that means that state of the connected bit (tag) is not read - reflected on the button. Does any know how to read the tag state and set it in Button when data is changed (e.g. from panel)? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/28/2022 09:24:12New subject after splitting Last edited by: C-3PO at: 03/28/2022 17:24:28If you find my contribution helpful please RATE it :)) |
|
Follow us on