2/25/2018 9:10 AM | |
Posts: 19 Rating:
|
Read bytes public byte[] ReadBytes(DataType dataType, int db, int startByteAdr, int count) This reads up to 200 bytes (actual limit of the protocol) from a memory location that you determine. What is S7.Net? S7.Net is a plc driver that works only with Siemens PLC and only with Ethernet connection. This means that your plc must have a Profinet CPU or a profinet external card (CPxxx card). S7.Net is written entirely in C#, so you can debug it easily without having to go through native dlls. Supported PLC S7.Net is compatible with S7-200, S7-300, S7-400, S7-1200, S7-1500. 1. Example: --Deleted link-- 2. Password: like share and subscribe video AttachmentS7.Net Tutorial.rar.zip (951 Downloads) |
Last edited by: Jen_Moderator at: 2/26/2018 10:02:17 AMDeleted link and added file as an attachment. |
|
8/9/2019 6:49 PM | |
Posts: 1 Rating:
|
Pass please |
8/9/2019 7:20 PM | |
Posts: 3093 Rating:
|
Did you try to download the file? |
9/2/2023 7:30 AM | |
Posts: 1 Rating:
|
thanks, i am looking for this method for almost one week! very helpful! |
Follow us on