5/27/2014 11:34 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Try it with Save As (with reorganisation). |
This contribution was helpful to4 thankful Users |
5/27/2014 9:12 PM | |
Posts: 60 Rating: (8) |
MESSAGE IS REMOVED BUT LED STILL SHOWING INTF ON PLC. |
This contribution was helpful to1 thankful Users |
5/28/2014 2:43 PM | |
Posts: 4 Rating: (0) |
I THINK INTERNAL DATA STRUCTURE IS SOLVED.BUT INT_F IS REMAINING. |
5/28/2014 4:52 PM | |
Posts: 559 Rating: (87) |
Have you checked the Battery of PS? Sometimes due to battery fault also it shows you IF. Check it out. |
This contribution was helpful to1 thankful Users |
5/28/2014 8:05 PM | |
Posts: 60 Rating: (8) |
YES I HAVE CHECKED BATTERY ALSO.BATTERIES ARE OK.BUT STILL INT_F |
5/28/2014 8:07 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
If you want send me the project...or attach here the recent diagnostic buffer messages list. |
5/28/2014 8:08 PM | |
Posts: 72 Rating: (6) |
What is showing in diagnostic buffer? |
5/29/2014 7:38 AM | |
Posts: 63 Rating: (4) |
It may be because of some wrongaddressing in programming, diagnostic buffer will let you know the prob more closely. |
Follow us on