5/18/2011 6:02 PM | |
Joined: 2/15/2010 Last visit: 1/20/2024 Posts: 329 Rating: (6) |
Dear, I am facing the same situation after power failure the mp277 touch shown this message Boot loader mp277-10 touch version 1.2 Date 26.06.2007 and not able to respond with pg shall somebody tell this software or hardware failure and if software shall somebody suggest how can i make factory resttings? and you have to know you can not see any thing at touch screen except the mentioned above message. Hope your fast reply because of i run line with my pg via run time wicc flexible. Regards, Splitted from MP277 is a brick after power loss during restore operation. Any hope?. |
Last edited by: O_Moderator at: 5/19/2011 8:45 AMnew subject after splitting Hazem |
|
5/19/2011 8:47 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151)
|
Dear hazem, You will have to perform an OS update with the option "Reset to factory settings" The earlier mentioned link descripes how to do. You will need a RS232/PPI multi master cable. When you perform an OS update with option "Reset to factory settings", you will be asked to boot the panel. After that the OS update will start. Edit: Here is mentioned link: how do you do an operationg system update (OS update) on operator panels? Best regards, Wizard |
Last edited by: Wizard at: 5/19/2011 8:49 AMLink added |
|
3/18/2012 6:23 AM | |
Posts: 13 Rating: (0) |
dear Hazem, I m facing the same problem. Please help me to resolve the same. Waiting for ur reply....... |
3/19/2012 11:34 AM | |
Joined: 4/29/2010 Last visit: 4/30/2024 Posts: 1557 Rating: (161)
|
Hi, all needed settings and also the instruction about reset a panel to factory settings can be found in this FAQ: How do you do an operating system update (OS update) on operator panels? best regards. |
Follow us on