8/12/2013 9:28 PM | |
Posts: 18 Rating: (0) |
thanks for your interest.. i try to select project name, but i can't compile or simulate or start the RT. neither for the client: when i try to simulate the client (with all the simulations in off and nothing running), TIA reports an error window saying "impossible to compile the selected object" and in the top of this windows there is the code 0125:000006. But if i try to compile the client it seems to compile right. In any case i don't find any .mcx with the client's name, only the server's .mcx. i tried to upload the project.. AttachmentProgetto1.zip (462 Downloads) |
Last edited by: sweetol at: 8/12/2013 9:43 PMLast edited by: sweetol at: 8/12/2013 9:32 PM |
|
8/12/2013 9:32 PM | |
Joined: 7/7/2010 Last visit: 1/24/2025 Posts: 15558 Rating: (2468)
|
Time to try Support Request |
science guy |
|
Follow us on