4/15/2010 7:07 PM | |
Joined: 9/23/2005 Last visit: 12/8/2023 Posts: 4284 Rating:
|
Hi, |
Denilson Pegaia |
|
4/16/2010 7:48 AM | |
Posts: 3 Rating:
|
Hello, V4.0.0.81 is not greater than the required V4.0.6 or greater. You have to update it. But there is now a libary available with a function block which can make a communication to a OPC - Server via GSM/GPRS modem SINAUT MD720-3 and send SMS through the modem. You find it here: http://support.automation.siemens.com/WW/view/en/39863979 BR Stefan |
4/16/2010 3:37 PM | |
Joined: 5/28/2008 Last visit: 12/1/2023 Posts: 1343 Rating:
|
I'm not quiete sure, but I think in this Example from Application&Tools is SMS sending included: http://support.automation.siemens.com/WW/view/en/39863979 regards EDIT: read to late, NLL-Stefan posted the same. thanks |
Last edited by: Robster at: 4/16/2010 3:38 PM |
|
7/30/2014 4:31 PM | |
Joined: 4/24/2009 Last visit: 11/23/2023 Posts: 2683 Rating:
|
New question was split to send flow level to seven segment display using s7-1200 plc with CM1241(RS485). Best regards O_Moderator |
7/1/2015 10:05 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4782 Rating:
|
|
Follow us on