1/17/2011 8:16 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello Experts, Recently new CNC lathe is installed in our shop with Sinumerik 802D, with 6SN1123-1AB00-0BA1 2x9A power module & 6SN1118-0NH11-0AA1 control module. AC servo motor 1FK7100-5AF-1AA2 I.E. 12 Nm, 8 A rated. Main spindle drive is AC induction motor of 55 Kw with Yaskawa drive. X axis is tripping on 380500 - fault code 608 value 0. we checked & found drive parameter 1105,Maximum permissible current, is set at 59 %. This parameter is pre-set at time of first start up. (Please find attached here with the description of current limit setting) My question is it tripping because of this P1105 parameter?. Also as per manual it is pre calculated at first power start up & for calculated for unlisted motor. Then in my case, when the complete package is of Siemens make why it is not getting updated as rated motor current? i.e. in my case as 8 Amp? Can any one help me?. Thanks in advance. DEEP. AttachmentCurrent limiting.pdf (446 Downloads) |
Last edited by: DEEPSTR2010 at: 1/17/2011 8:18 AM |
|
1/21/2011 5:17 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello Experts, is something wrong or my question isn't clear? DEEP. |
Follow us on