8/10/2010 8:02 PM | |
Joined: 6/29/2010 Last visit: 10/27/2022 Posts: 112 Rating: (63) |
Hi, In the properties of the message text, click on the weekly timer, at your right will appear the settings available to insert in message text, click on the parameter and click on insert parameter button. AttachmentWeekly Timer.zip (835 Downloads) |
8/12/2010 3:10 PM | |
Joined: 6/29/2010 Last visit: 10/27/2022 Posts: 112 Rating: (63) |
Hi, You only can change the program by display of LOGO! module or by LOGO! Soft Comfort. In LOGO! TD you can change parameters added in messagem text of your program. To change parameters in LOGO! TD, you have to press "esc" button for 3 seconds, when the cursor appear, you can select the parameter to change pressnig the "right arrow", then you can change the parameter selected pressing the "OK" button and pressing arrow up or arrow down to change values in the position of the parameter. Attachmentweekly timer with program.zip (761 Downloads) |
Last edited by: MrPaiva at: 8/12/2010 3:11 PM |
|
This contribution was helpful to1 thankful Users |
8/12/2010 10:22 PM | |
Joined: 6/24/2010 Last visit: 12/7/2021 Posts: 21 Rating: (2) |
Maybe this will help if you need to change all three cams. Press F1 to toggle through the cams. Regards, Richard Attachmentweekly timer in TD all 3 cams.zip (748 Downloads) |
This contribution was helpful to1 thankful Users |
10/18/2012 6:17 PM | |
Posts: 8 Rating: (0) |
how can I do to change ON time and OFF time for weekly timer (cam 1) using Network Analog Input?? |