2/12/2014 9:55 AM | |
Joined: 2/12/2014 Last visit: 5/28/2023 Posts: 158 Rating:
|
How to simulate a PLC using a CPU 1214 s7-1200? I use TIA PORTAL V12 |
2/12/2014 10:16 AM | |
Joined: 2/12/2014 Last visit: 5/28/2023 Posts: 158 Rating:
|
Thank you. Dear hdhosseini, I've tried the S-300, the digital inputs can be simulated, but the S-300 there are no analog inputs. Is there a CPU that has analog inputs and can be simulated? |
2/12/2014 10:35 AM | |
Joined: 1/28/2009 Last visit: 12/4/2023 Posts: 6824 Rating:
|
Hello, If you are using TIA Portal, it is possible to simulate S7-300 CPUs with PLCSIM.You can find all ranges of variables that you can work with in the user interface(Digital Inputs,Analog Inputs,Memories,Timers,...).I suggest reading the PLCSIM manual for effective use of it. Read section "5.5 Input Variable View Object " of this manual. S7-PLCSIM Best regards, Hamid Hosseini |
This contribution was helpful to
1 thankful Users |
2/12/2014 11:08 AM | |
Joined: 2/12/2014 Last visit: 5/28/2023 Posts: 158 Rating:
|
thank you very much. sorry I didn't read carefully, the S-300 313C module has analog inputs. |
Follow us on