8/15/2013 9:44 PM | |
Joined: 9/23/2005 Last visit: 1/22/2025 Posts: 4396 Rating: (1464)
|
Hi, do you need a open a V11 SP2 project in V12 and from there upload the PLC. See How do you load the project data from the CPU into the programming device in STEP 7 (TIA Portal)? |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
8/18/2013 4:48 PM | |
Joined: 1/10/2013 Last visit: 10/13/2023 Posts: 12 Rating: (0) |
Hi thank you. It works now
|
8/19/2013 12:33 PM | |
Joined: 9/23/2005 Last visit: 1/22/2025 Posts: 4396 Rating: (1464)
|
You are wellcome :) |
Denilson Pegaia |
|
2/13/2014 8:26 AM | |
Posts: 340 Rating: (6) |
new question is splittet to is it possible to upload and save data in tia program with hardware configuration?. |
2/22/2015 2:42 AM | |
Posts: 2 Rating: (0) |
Hello, have exactlly the same problem. Guess need to install some updates? The link provided by Pegaia doesn't work any more. Pls., assist |
2/22/2015 3:00 AM | |
Posts: 2 Rating: (0) |
hello, have the same problem. but link doesn't exist anymore. Could you assist pls. Pop-up window tell me: The program on the CPU is incompatible with the Step7 proj. Version of the program on the CPU:V11 ----Version on the Step7 proj V12 Thank you |
11/4/2015 12:30 PM | |
Joined: 8/21/2014 Last visit: 1/23/2025 Posts: 1036 Rating: (14) |
New question published by AutoGen_578662 is split to a separate thread with the subject Try to open V11 Projekt in V13. Best regards |
My Forum is the place to personalize your profile, |
|
10/13/2016 10:04 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by Xurshid is split to a separate thread with the subject Upload TIA V12. Best regards |
Follow us on