12/14/2009 9:50 PM | |
Joined: 3/14/2008 Last visit: 1/17/2025 Posts: 2161 Rating:
|
Hello, I have a PID with for example the following parameters: SPEXT, SPEXT_ON, PV_IN, LMNR_IN I'll pick this block from the PCS7 library(using single user project) and then put it in CFC and then customize it with my chosen parameters. If I need three more PID blocks with also the same parameters, how can I make sure that I get the same customised block again? If I just get it from PCS library, I will get the standard block obvious. I think I have to create a personal library, but what are the correct steps to be taken? TThx |
If I could help you, you can use the RATE button. Thank you. |
|
12/19/2009 8:20 PM | |
Joined: 3/14/2008 Last visit: 1/17/2025 Posts: 2161 Rating:
|
Dear Smiffy, That is what I meant. If I use digital drivers and I want to hide a few parameters, then I have to do that for 1000 I/O. So one time creating the driver block with only the parameters I need, and then use it for the remaining I/O. You explained it right. Thx! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on