11/13/2020 4:52 PM | |
Joined: 1/17/2020 Last visit: 10/8/2024 Posts: 46 Rating: (6) |
Hi, In Runtime, the user acknowledges an alarm in one of the following ways, depending on the configuration:
Configuring a button to acknowledge an alarmTo configure a button for acknowledging an alarm, proceed as follows:
|
Last edited by: Krono314 at: 11/13/2020 16:55:17Rate please if it was useful! |
|
11/17/2020 6:35 PM | |
Joined: 3/30/2020 Last visit: 10/8/2024 Posts: 4828 Rating: (988) |
Hello. Attached is an example for Step7 Basic V14 and WinCC Basic V14 that can be simulated. This one is worth BitCoin. Not only does it demonstrate the alarm acknowledgement but it also contains helpful notes in OB1 and the HMI pages. Some secrets are also made clear by x3 examples. I hope you find plainly worded and useful. Regards. Attachmenthmi_alarm_ack_TIA14_V0.zip (579 Downloads) |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to2 thankful Users |
Follow us on