3/19/2018 6:21 PM | |
Joined: 2/18/2015 Last visit: 1/16/2024 Posts: 66 Rating:
|
Hello I am working with a PLC S7-1200, CPU 1214C DC/DC/DC . I want to read both count and frequency in the same High Speed Input. The configuration that I need is the following:
The thing is that I need exactly 6 HSC reading both count and frequency. Therefore, it is not possible for me to use 2 HSC for one encoder (one for count and the other for frequency). My question is if this is possible to read both count and frequency in the same High Speed Input? If not, I know I would need a ET200 and counter cards. In that case, What are the models of the ET200 and counter card that are compatible with a S7-1200. Thanks in advanced. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/20/2018 9:05:55 AMNew subject after splitting |
|
Follow us on