1/12/2007 8:31 AM | |
Joined: 9/28/2005 Last visit: 10/24/2024 Posts: 414 Rating: (28) |
Hi, May be there is some hope,I found some information about a USB to PCMCIA converter. |
Smurf |
|
1/12/2007 8:49 PM | |
Posts: 324 Rating: (30) |
Hi Smurf, have you read the content of the Page? There it is written that only all 16 PC Cards are supported, but the 32 Bit Cardbus Cards are still under development, see for yourself: "This can be any standard or custom 16-bit PCMCIA card (Type I, II, or III). Just for your information the CP 5512 is a Cardbus Adaptor.... only a CP 5511 is a PCMCIA Card (16 Bit). Best regards Calm_down |
4/26/2007 5:02 PM | |
Posts: 7 Rating: (2) |
Hi there, As it seems, the following adapter works fine. Also on PROFIBUS slave modules. http://www.duel-systems.com/products/CategoryDatasheet.aspx?id=4 |
9/22/2007 4:30 PM | |
Posts: 115 Rating: (1) |
Dear Michaelk, If your operating system recognize the USB-PCMCIA adapter ,in my mind it should work and you can use CP5512. Saeed |
9/23/2007 10:45 AM | |
Posts: 7 Rating: (2) |
Hi there! USB can do the job but as far as I know, you cannot connect to PROFIBUS slaves! As we all know the 5512 is the perfect card to programm with. I have found a simple solution: http://www.duel-systems.com/products/adapters.aspx It works fine, not very expensive!!! use it! Not plug & pray, it really works |
Follow us on