11/16/2017 2:50 PM | |
Posts: 17 Rating:
|
Durius, One last question: I don't know how to use pointers to store the data readed from the slave. So I want to use a block of MB_Client with different "data_prm" for each kind of read data. In this case, it would be 4 blocks, one for each type of registers (coil, discrete input, holding registers, input registers), but all the 4 blocks, reading data from the same slave. Even in this case, do i not need to use the disconnect option? All four blocks must use the same connection ID and instance DB? Thanks for the help! Best regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/17/2017 7:26:11 AMNew subject after splitting |
|
11/17/2017 11:28 AM | |
Joined: 4/28/2015 Last visit: 3/26/2025 Posts: 10837 Rating:
|
Hello, also this topic can be very helpful for another solution - Variant definition |
With best regards... |
|
Follow us on