12/19/2023 8:47 AM | |
Joined: 8/3/2009 Last visit: 4/30/2025 Posts: 15403 Rating:
|
Hello hewking103 IN the IM folder there are stored all generated RUntime tdata and also some other data for example serach index and so on. Everything will be generated by TIA new: https://support.industry.siemens.com/cs/de/en/view/109778709 -> the SAS DC tool works also for WInCC Prof: LINK You should set up your stations alsways with this FAQ: LINK
But there are so many possible real problems or even normal behaviour that you would see as a problem that you cannot give a general troubleshooting guide Post details if your have questions in this forum or create a Service Request at Support if you need quick and critical help Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
12/19/2023 11:00 PM | |
Joined: 1/20/2022 Last visit: 1/10/2025 Posts: 369 Rating:
|
hi Murof Thanks for reminding about data collection tool. Your links are very useful and bookmarked.
|
Follow us on