5/16/2019 8:58 AM | |
Posts: 14 Rating: (0) |
Good morning, Sorry I don't want to Interrupt your topic. My topic is also regarding with this subject. That's why I am posting my question here. I have LOGO! 6ED1055-1MA00-0BA2 device. How do I wire this 4 wire potentiometer to logo. basically 4 colour wires are here. My condition is to Stop the Motor at certain distances. For eg: I have to stop the motor at 250mm. My planning is to connect this potentiometer to the motor. So that, when ever the motor works the potentiometer also pulled out and give a reference voltage from 0-10. How can I perform this. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2019 11:04:42New subject after splitting |
|
5/17/2019 11:13 AM | |
Posts: 14 Rating: (0) |
|
5/17/2019 11:33 AM | |
Posts: 14 Rating: (0) |
how can i check that? |
Follow us on