2/28/2023 8:22 AM | |
Joined: 9/3/2008 Last visit: 4/11/2025 Posts: 933 Rating:
|
Hi, Based on your description, I have made a sample that does what I think you want. See the attached two printscreens in zip file. They show a sample script with one start screen containing two picture Windows (called "scrWin1" and "scrWin2"). In each Window is a picture "page1" and "page2". In page1 are two buttons containing the same c-script. One sets the IO field "Visible" property to FALSE, the other to TRUE. Printscren 02-page1clickevent.PNG show the script that sets it to invisible. I hope it helps. Attachmentcscript.zip (258 Downloads) |
Michael |
|
This contribution was helpful to
1 thankful Users |
2/28/2023 1:59 PM | |
Joined: 3/25/2008 Last visit: 4/17/2025 Posts: 240 Rating:
|
A thousand thanks . It's exactly what I was looking for. You solved a big problem for me Thank you again Fabio |
Follow us on