3/6/2025 10:19 AM | |
Joined: 12/26/2024 Last visit: 4/26/2025 Posts: 2 Rating:
|
Hello Everyone, Hope all doing well. I have a problem related to property instance as BOOL type. So, I made a button in which I defined some bool tags in property interface like Sheet, Sheet_1, Sheet_2, Sheet_3 up to Sheet_8. So, here I want to Set value of Sheet=1 and From Sheet_1 to Sheet_8=0.Note that here I am using property interface I am not using tags interface. If I define event that I can't access the instances of property interface directly. So please help me for this issue. AttachmentButton Event Issue.xlsx (14 Downloads) |
Follow us on