6/19/2008 8:52 AM | |
Posts: 1776 Rating:
|
Hi, no problem see FAQ http://support.automation.siemens.com/WW/view/en/23711489 |
6/30/2008 11:56 AM | |
Posts: 1776 Rating:
|
Hi, you can not use a WinCC project edited with WinCC V6.2 with WinCC V6.0. WinCC is not downwards compatibel see FAQ http://support.automation.siemens.com/WW/view/en/21927773 WinCC generally upwards compatible. This means that if, for example, you have upgrades WinCC V6.0 to WinCC V6.0 SP4, you can also operate your WinCC V6.0 project with WinCC version V6.0 SP4. You can find notes on this in the "Migration" chapter in the WinCC Online Help. |
Follow us on