Industry Online Support
Technical Forum
10/13/2006 6:03 AM | |
Joined: 5/19/2006 Last visit: 12/3/2024 Posts: 549 Rating: (107)
|
Have you seen this post? Dec |
10/13/2006 8:29 AM | |
Posts: 9 Rating: (0) |
Thanks, But None of the list problem is my problem Any Suggestion for this. Thanks |
10/13/2006 10:27 AM | |
Posts: 1776 Rating: (95) |
Hi, Is Your installation Ok? Have You checked the Install Notes? Have You checked the Event Logs? Maybe the link will also help http://support.automation.siemens.com/WW/view/en/22127699 |
10/13/2006 2:16 PM | |
Posts: 1084 Rating: (72)
|
Hi, Try to log on as on as a local administrator (if you did not do that already) and see if that helps. Did you also read this faq? Keep us posted of the outcome. with regards, ikkezelf |
10/16/2006 9:01 AM | |
Posts: 9 Rating: (0) |
Hi, May be Its better I give hsytorical description about my PC. 1. I Install PCS 7 System (With WinCC Sp3 + SQLServer 2000 SP3) --> No Problem. 2.I Uninstall PCS7 System --> No Problem. 3.I InstallWinCC Sp3, SQL Server 2000 SP3, Step 7, PLC Sim --> No Problem. 4. I Uninstal (WinCC Sp3 + SQL Server 2000 SP3). 5. I Install Industrial Application Server 2.1 + SQL Server SP3a (with not default directory) (For The project) --> No Problem. 6. I Install WinCC SP3 + SQL Server 2000 SP3 (With default directory) --> No Problem. 7.OpenExisting Project WinCC --> Hresult Error, 0x80046127 : (null) 8. I Uninstall IAS 2.1 and WinCC SP3 (with database) and Clean Regedit (WinCC Folder). 9. I Install WinCC Sp3 + SQL Server 2000 SP3 (With default directory) --> No Problem. 10. OpenExisting Project WinCC --> Problem With the same message above. 11. Create New Project --> Problem With the same message above. 12. I Uninstall WinCC Sp3 + SQL Server 2000 SP3 and Clean Regedit (WinCC Folder). 13. I Install WinCC SP4 + SQL Server 2000 SP4 (With Default Directory). 14. Create New Project --> Problem With the same message above. Herewith, I give the Citamis.str file. Thanks for the support AttachmentCitamis.zip (395 Downloads) |
Follow us on