3/26/2023 7:45 AM | |
Joined: 3/30/2020 Last visit: 6/9/2023 Posts: 3579 Rating:
|
It would be best to consult the manual first. You did not mention which PLC you are using. Regardless, the following manual will already be helpful. LINK: SIMATIC S7 S7-1200 Programmable controller
2) Please rephrase the question. It is not clear what the question is about. 3) The HSC's counter value is presented in a DINT value. There is a transition between + and - when the range is overrun. Proper coding techniques can handle the situation so that detecting the overrun is not an issue. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on