4/27/2016 10:01 AM | |
Joined: 12/15/2015 Last visit: 5/31/2016 Posts: 147 Rating: (3) |
Hello Basically, when a client requires pulse inputs for a flow meter signal that means HSC inputs, right? What is the difference between PosInp(a module in the catalog), Count(a module in the catalog) and HSC (a feature in the HF DI module)? So if I select the S71500 32 HF DI module (6ES7 521-1BL00-0AB0) , it will have 2 HSC inputs with 1 khz frequency. (please find attached image) Did I understand that right? If yes, if I have the requirement of 8 Pulse input, that will mean I will have to buy 4 HF modules (4 HF modules x2 HSC each = 8 HSC) or is there a better option to go with? and would the HSC inputs here be the first 2 bits? because in TIA V13 SP1 hardware configuration there is nothing special in the configuration for those 2 inputs (paramatrization) Thank you ------------------------------------------------------------------------------------------ |
Last edited by: AUTOMOTO21 at: 4/27/2016 10:09:57 AMLast edited by: AUTOMOTO21 at: 4/27/2016 10:10:40 AMLast edited by: AUTOMOTO21 at: 4/27/2016 10:11:48 AMLast edited by: AUTOMOTO21 at: 4/27/2016 10:13:21 AMLast edited by: Min_Moderator at: 4/28/2016 12:13:54 PMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
4/27/2016 10:49 PM | |
Posts: 5225 Rating: (1192) |
I wondered if a search in this forum would deliver something.. I found these for you:
I suggest you get yourself a COMPACT type PLC. There you have x6 HSC already available as part of the PLC. Thereafter you will have to use technology modules. Note also you may require the use of Technology Objects too. Cheers. |
Last edited by: William_B at: 4/27/2016 10:50:52 PMPS: I recommend you start a new question next time.. your question looked very much like a statement to me in this thread. |
|
4/28/2016 9:34 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi AUTOMOTO21, for pre-sales questions Siemens has a technical consulting/engineering support. You can find your local Siemens contact in Contact database: Your Personal Contacthope this helps, regards, |
FCK WAR! |
|
4/30/2016 6:02 PM | |
Joined: 12/15/2015 Last visit: 5/31/2016 Posts: 147 Rating: (3) |
Thank you very much for your detailed answer WilliamB, and thanks alot for the screenshots they are really helpful. One more thing I would like to ask please. for 9 flowmeters do I need to purchase 5 modules of those? (5 modules x 2 pulse inputs = 10 inputs) or is there a better solution like a card that has more high speed inputs? Thank you edit: attached the data sheet of the flowmwter just in case Attachmentflowmeter data sheets.pdf (612 Downloads) |
Last edited by: AUTOMOTO21 at: 4/30/2016 6:07:16 PMLast edited by: AUTOMOTO21 at: 4/30/2016 6:19:13 PM |
|
Follow us on