11/21/2021 5:13 PM | |
Joined: 5/30/2016 Last visit: 11/30/2022 Posts: 5 Rating:
|
Hello, Could anybody help me to find HSP s71200 v4.5 for TIA16. I purchased new controller 6ES7214-1HG40-0XB0 with firmware v.4.5.0 inside But similar controller which I can see in my TIA16, with latest frm, is v.4.4. Thanks beforehand. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/22/2021 05:47:33New subject after splitting |
|
11/21/2021 5:48 PM | |
Joined: 12/18/2014 Last visit: 2/8/2023 Posts: 29119 Rating:
|
There is no HSP for V4.5 in TIA V16. If you want to all functions of V4.5 you need TIA V17. |
11/21/2021 5:54 PM | |
Joined: 12/18/2014 Last visit: 2/8/2023 Posts: 29119 Rating:
|
But you can work with TIA V16 an d a CPU with firmware V4.5x. |
11/21/2021 6:26 PM | |
Joined: 3/28/2015 Last visit: 2/7/2023 Posts: 698 Rating:
|
Hello, Have a look at the following topic: Release S7-1200 CPU Firmware version V4.5 ---------------------------------------------------------------------------------------------------- 1-The new firmware version can be loaded on any S7-1200 hardware with a firmware version V4.0 or later. 2-To configure the SIMATIC S7-1200 CPUs version 4.5 and higher it requires the Engineering System Step7 with version V17.0 and higher, Basic or Professional. SIMATIC Step7 Safety Basic or Advanced V17 is required for Failsafe CPU types. 3-An S7-1200 CPU with version 4.5 is replacement compatible with an S7-1200 and firmware version 4.0, 4.1, 4.2, 4.3 and 4.4. This enables the use of a real existing CPU with firmware version 4.5 with an engineered V4.0, V4.1, V4.2, V4.3 or V4.4 based on an existing TIA portal older versions project. The new firmware features cannot be used in that case. ------------------------------------------------------------------------------------------------------ |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
2 thankful Users |
11/21/2021 8:34 PM | |
Joined: 5/30/2016 Last visit: 11/30/2022 Posts: 5 Rating:
|
Thanks for reply, but it sounds not so good. Are there any ways to downgrade cpu firmware till v.4.4? |
Follow us on