3/30/2022 5:22 PM | |
Joined: 3/30/2022 Last visit: 4/14/2022 Posts: 2 Rating: (0) |
Hi, i wonder if anyone can give advice, i have a Hydro ranger 200 six relay model, it will accept two ultra sonic heads and has two 4-20ma outputs. The installation i am working on has one u/s head installed and one 4-20 output used. i would like to programme the second 4-20ma output to the same value as the first, ive been through the manual and im struggling to find the correct menu to enable and assign the output. Any help would be appreciated. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/31/2022 09:51:52New subject after splitting |
|
Follow us on