5/18/2014 1:20 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
I do not have the panel, and I have no connected any start signal. How can I give a stop? Hi is in ready not runing.. |
5/18/2014 1:22 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello, Does your drive has AOP? |
5/18/2014 1:24 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
No |
5/18/2014 1:29 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
When i cut the 400V power supply, inverter is off |
5/18/2014 1:29 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello, Then how start (run), stop & set point is applied to drive? |
5/18/2014 3:14 PM | |
Joined: 5/10/2013 Last visit: 10/16/2023 Posts: 11 Rating: (0) |
I start inverter then i give stop ( from Starter) and still cannot change this parameters |
5/18/2014 3:47 PM | |
Joined: 1/21/2013 Last visit: 6/2/2024 Posts: 4620 Rating: (705) |
Hello, And the led on the front of MM4 (green and yellow) as they are? (Flashing,fixed)
|