Industry Online Support
Technical Forum
3/16/2011 3:03 PM | |
Posts: 14 Rating:
|
Thanks! I have an other problem with this system. I have also a WinCC SCADA system that comunicate with H PLC in industrial ethernet. I have just setted up communication between PC and PLCs but in this way I can not communicate between TP177 and PLC. TP177B works only via TCP/IP PC works only via Industrial Ethernet. Splitted from TP177B Redundant connection. |
Last edited by: O_Moderator at: 3/17/2011 8:56 AMnew subject after splitting |
|
3/18/2011 8:44 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, if you what to connect this panel also to the H-CPU, maybe this faq can help you: How do you connect a panel to a SIMATIC H station? best regards |
Follow us on