2/18/2011 8:56 AM | |
Joined: 12/9/2010 Last visit: 9/19/2023 Posts: 162 Rating:
|
So a new problem accured. I'm transfering batch numbers between my CPUs and these consist of Letters and Numbers. I think the correct data type for this is the STRING. Is that correct? If so, my problem is that I can't place a STRING data in my data block in the STRUCT. If I have understood this correctly it is in the STRUCT of my data block I shall place the data to be transfered over the ethernet communication. If I use a second TSND_C and TRVC_C block in my CPUs to transfer the STRING seperatly, is it possible to make them work together so that the information come to the right place. TSND_C 1 to TRCV_C 1 TSND_C 2 to TRCV_C 2 The information in TSND_C 1 shall not be transfered to TRCV 2.
Understand my questions? I will be thankfull for any suggestions Regards /Tim Splitted from s7 1200 - s7 1200 ethernet connection Rcv and Send. |
Last edited by: O_Moderator at: 2/21/2011 7:55 AMnew subject after splitting |
|
2/23/2011 6:02 PM | |
Joined: 12/9/2010 Last visit: 9/19/2023 Posts: 162 Rating:
|
I will do this at work tomorrow, sorry for late reply, I had alot to do today. |
Follow us on