12/17/2015 2:56 PM | |
Joined: 3/26/2009 Last visit: 8/27/2024 Posts: 29 Rating:
|
Hello, I am having a hard time getting this communication to work. Basic setup: 1517-3 PN/DP is the IO controller I tried many different solutions, nothing works. At the moment I have the S7-319 acting as the iDevice, setup in Simatic Manager. Exported the gsd file and setup the 1517 in TIA portal with the gsd file as idevice. The PLCs act normally, no faults. But I cannot get any data from to the other. Can anybody point me in the right direction? In the end I have to communicate with the CP343-1, not with the 319 directly. AttachmentStep7_300.zip (554 Downloads) |
12/18/2015 10:00 AM | |
Joined: 5/12/2006 Last visit: 3/25/2025 Posts: 22600 Rating:
|
Hello, in the S7-1500 i use no blocks. In the S7-300 the blocks from you are running.
Christoph |
Follow us on