3/25/2016 4:26 PM | |
Posts: 2 Rating:
|
I have 2 cpu 315 2NP/DP comunication betuin via Ethernet? Comunication 2 cpu Please Example |
3/25/2016 11:48 PM | |
Joined: 9/27/2006 Last visit: 4/29/2025 Posts: 12347 Rating:
|
Hello moris; There are many ways that these 2 CPUs can exchange data over their integrated Profinet port: - S7 connections (GET/PUT, BSend/Brecv...) - TCP/IP (TCOnn, TDISC...) - Modbus/TCP (with special licensed blocks see https://support.industry.siemens.com/cs/ww/en/view/22660304) - Profinet This document will help you understand all the types of communication you can do with your 2 PN CPUs (it requires a bit of study, though): CPU-CPU communication with SIMATIC controllers (compendium) https://support.industry.siemens.com/cs/ww/en/view/20982954
Easiest would be Profinet (it is supported natively by the integrated ports of your CPUs and requires mostly configuration), where one CPU would act as a Profinet IO controller and the other as a Profinet I-Device. The following Application example will explain how to plan and configure this connection: PROFINET IO - Configuration & Diagnostics https://support.industry.siemens.com/cs/ww/en/view/22981197 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/25/2016 11:49:09 PM |
|
3/26/2016 7:45 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
Hi See the links provided in this thread Regards Manmeet |
Follow us on