1/31/2011 8:06 AM | |
Posts: 1 Rating:
|
Hi Kevin, I have a AK1703 and I want to communicate Sinamics s120 (VFD)through profibus communication. I have toolbox II to configure the same and i tried to but without success. I require a GSD file for SM2545 to configure the hardware and the CP i use is CP2017. Also tell me about SYCON please. Kindly help me in configuring this. thanks, Sathish Kumar.S Splitted from AK 1703 ACP configuration. |
Last edited by: O_Moderator at: 1/31/2011 9:23 AMnew subject after splitting |
|
5/21/2014 3:10 PM | |
Joined: 11/21/2007 Last visit: 2/7/2023 Posts: 2321 Rating:
|
Hello rchie You can download the GSD Files for G120 from the following link : SINAMICS G120: PROFIBUS GSD files Always use the GSD file that matches your Control Unit (CU) type or order number – even if you are currently not using all of the Control Unit functions. The GSD FIles have all the functions required for Drive Operation / Monitoring from a Profibus Master. You will have to do the matching settings in the Drive also using Drive Starter ( e.g. Profibus address , Communication Profile etc.. ) Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on