8/25/2017 9:26 PM | |
Joined: 7/11/2013 Last visit: 1/3/2023 Posts: 2 Rating:
|
Hi I have the same problem. If I have a firmware 4.2.1 and tia portal v13, the plc works fine?. Becouse I have a config. 1214c + sm1223 and all the input appear in false state. When its connected to 24v. Regards. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/6/2017 4:02:34 PMNew subject after splitting |
|
8/26/2017 2:31 AM | |
Posts: 1529 Rating:
|
You have another problem other than firmware. You have a wiring error. The inputs read "1" perfectly well in all software version since Beta 0.1. |
Follow us on