Industry Online Support
Technical Forum
9/12/2012 9:41 AM | |
Joined: 7/8/2012 Last visit: 3/24/2022 Posts: 13 Rating: (0) |
Hi, I have a problem with my INSYS GSM 4.3 LOGO!. it is not talking with my LOGO. I tried number of ways. When i given an alarm input to INSYS it is given the replay, but when i connected with Logo and run the program the Insys not responding. RX/TX is not flashing. I tried the way that i given a "STATUS?" sms to INSYS then that RX/TX LED is just blinked and Status LED is blinked three times. But i didnt get any response back.. I have checked the history in that it is showing 'GSM ERROR'. My LOGO Part number : 6ED1 052-1FB00-0BA0 My LOGO PC Cable part No : 6ED1 057-1AA00-0BA0 Please check the attached Insys settings also.
AttachmentInsys.zip (211 Downloads) |
Last edited by: O_Moderator at: 9/14/2012 10:09 AMnew subject after splitting from /tf/WW/en/Posts/15736#top |
|
9/14/2012 10:13 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread INSYS GSM is not talking with my LOGO Best regards O_Moderator |
Follow us on