6/21/2010 9:58 AM | |
Posts: 2 Rating: (1) |
Hi everyone Please help me. I have a problem with WinCC Flexible 2008 Advance SP2. I'm using WinCC Flexible 2008 SP2 Advance, Sometimes, I meet this case: I use WinCC Flex to open a project which programed and compile ok(before i still open it normally), at the moment I can open it but i can't see anything, a empty screen like following attached file. I try to open others project, create a new project but still meet the same situation. Before, I met this situation and I must re-install it. you know re-installing is tired. How must I do to see normally? please help Thanks a lot Van Don Splitted from WinCC Flex 2008 and PLC SIM V5.4. |
Last edited by: O_Moderator at: 6/21/2010 10:18 AMnew subject after splitting |
|
6/21/2010 3:57 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Hello, Before reinstalling WinCC Flexible 2008 SP2 you can try to do something you'll find in attached file. Just right click on the Flexible icon near the clock and make 'reset settings'. If this will not help then reinstall only service pack 2. Its lees painful and normally should be enough. Please also check the compatibility list to avoid any conflicts in the future. You'll find list here. |
Best regards, |
|
This contribution was helpful to3 thankful Users |
6/22/2010 12:58 PM | |
Joined: 9/5/2007 Last visit: 3/7/2023 Posts: 317 Rating: (17) |
You're welcome |
3/20/2018 1:58 PM | |
Joined: 6/19/2017 Last visit: 4/19/2024 Posts: 7945 Rating: (162) |
New question published by aleegauhar1 is split to a separate thread with the subject Want to connect 50 PLCs s7-300 315-2dp CPU to a central pc over an Ethernet network - Is there any other limitation in wincc flexible 2008 advanced?. Best regards |
Last edited by: Jen_Moderator at: 3/20/2018 2:01:41 PMOptimized headline. My Forum is the place to personalize your profile, |
|
Follow us on