4/10/2011 5:33 AM | |
Joined: 12/11/2009 Last visit: 9/8/2022 Posts: 243 Rating: (4) |
Hello I'm converting my logo project to s7-300. indeed plc prog is not very complicated but one network looks strange RS SF016 and RS SF029 How should I make it in s7 simatic manager? thanks Attachmentosman_logotos7300.zip (364 Downloads) |
4/10/2011 9:53 AM | |
Posts: 153 Rating: (15) |
Hi Osman I see two variants. 1) Programs for converting don't exist from LOGO in the s7 manager. This converting to do manually with use the LAD. RS SF016\RS SF029 is possible to construct by means of two logic elements. Look a picture. 2) To wait summer. And to familiarize with functions of LOGO Ethernet interface. But I can tell nothing as the network will work. (https://www.automation.siemens.com/tf/WW/en/Posts/54795#top ) |
Last edited by: Andres [Str] at: 4/10/2011 9:55 AM |
|
4/11/2011 2:16 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714) |
The s7300 has a RS function too, see pdf. Best regards, Marcjan AttachmentPrinting _RS _ Reset_Set Flip Flop.pdf (290 Downloads) |
Problem solved? |
|
4/22/2011 7:31 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Look at attachment. |
4/23/2011 7:19 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Yes, it's my fault. Should be RS. In my case is "Blagodarq", means Thank You. Best regards, Hristo Mihalev |
Follow us on