9/30/2018 12:20 PM | |
Posts: 1 Rating:
|
나는 t7 v3에서 s7-300을 사용하려고합니다. 저는 cp-341을 사용하여 modbus_master를 사용하여 타기와 통신합니다. 가능한지 여부를 알려주세요. 예를 얻을 수 있습니까? 고맙습니다. ------------------------------------------------------------------------------------------ |
Last edited by: 일월풍운 at: 9/30/2018 12:25:19 PMLast edited by: 일월풍운 at: 9/30/2018 12:26:12 PMLast edited by: The Helping Hand at: 10/1/2018 9:18:55 AMNew subject after splitting |
|
9/30/2018 2:23 PM | |
Joined: 9/27/2006 Last visit: 3/21/2025 Posts: 12344 Rating:
|
Hello Lunar Weather; There are many discussions and examples available on the forum for a CP 341 programmed as Modbus Master. The function you are referring to unfortunately applies only to S7-1200 and S7-1500 CPUs, not for S7-300 with a CP 341. You must use the functions designed especially for the S7-300/400 CPs as Modbus master (as shown in the following example.). In order to provide more information to you, we must know more details of the programming software you plan to use. Here is an application example for TIA Portal: ;Sample program MODBUS Master (standard block) zXX21_04_PtP_Com_MODMA.zip for STEP 7 (TIA Portal) https://support.industry.siemens.com/cs/ww/en/view/99742134 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/30/2018 2:24:24 PM |
|
This contribution was helpful to
1 thankful Users |
10/2/2018 2:50 PM | |
Joined: 8/3/2009 Last visit: 3/21/2025 Posts: 15056 Rating:
|
Hello Look here at chapter 57: https://support.industry.siemens.com/cs/ww/en/view/78028908 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on