9/28/2010 6:32 AM | |
Posts: 7 Rating:
|
Dear Experts, I am using CP341 as a Modbus slave to communicate with ABB PLC which is master. Distance from modbus slave to master (ABB PLC) is 1600mtrs. ABB PLC is using TCP-IP (OPC) to communicate with all vendors. For thiscommunicationIneedrepeater-cum-convertor which willconvertModbus RS485 protocol to normal TCP-IP protocol; this will be placed in center at 800mtrs. Please suggest me,is there anyconvertor available? & whether this communication is possible or not? Splitted from CP341 MODBUS reapeter. |
Last edited by: O_Moderator at: 9/28/2010 12:02 PMnew subject after splitting |
|
9/28/2010 5:50 PM | |
Joined: 1/17/2007 Last visit: 3/10/2025 Posts: 1557 Rating:
|
Lantronix do a very good one called XPress-DR-IAP. I have used it and I have to say it is very good. |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
9/30/2010 7:32 AM | |
Posts: 7 Rating:
|
Dear all, |
Follow us on