11/18/2015 4:43 PM | |
Joined: 4/8/2015 Last visit: 8/26/2024 Posts: 10 Rating: (0) |
Hi everyone, I'm having the same problem. I need to get the GroupName of each user on my WinCC project. Did anyone have the solution? Best regards, Ludson Farah ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/19/2015 11:17:54 AMNew subject after splitting |
|
3/19/2018 3:00 PM | |
Joined: 9/19/2009 Last visit: 12/23/2024 Posts: 459 Rating: (85) |
Hi If you want, you can try this library. The function string : GetUserGroup (string DataSourceRT, string CurrentUser)
Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
3/21/2018 4:49 PM | |
Joined: 9/19/2009 Last visit: 12/23/2024 Posts: 459 Rating: (85) |
Hi Vega I have update the library, if you work with Simatic Logon the users are from the OS, and not from WinCC, this is the reason the function doesn´t works. Can you tried this new function?
Regards
|
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on