5/18/2017 1:22 PM | |
Posts: 6 Rating:
|
I am using S7-300 CPU 313C-2DP communicate with CP343-1 and IM-153-4 profinet communication is established now the problem is that I/O's is not processing. When we high the physical input but is not showing on variable table. Is it any functional block need to call or some other configuration still required? If functional block need to call kindly suggest the FB/FC? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/18/2017 1:46:47 PMNew subject after splitting |
|
5/18/2017 1:36 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Faizan Taufig, yes, for profinet-communication with a CP343 you need some blocks to read out the I/O´s from the CPs profinet. this FAQ may help you to understand: How do you program communication blocks FC11 and FC12 for the PROFINET IO controller? hope this helps, regards, |
Last edited by: mopS04 at: 5/18/2017 1:36:48 PMFCK WAR! |
|
This contribution was helpful to
1 thankful Users |
5/20/2017 10:04 AM | |
Posts: 6 Rating:
|
Thanks I want to ask one more thing that how many I/O's can be configured to profinet? I need to connect 10 Di card 5 DO card and some analog |
Follow us on