1/6/2013 5:27 PM | |
Joined: 3/21/2006 Last visit: 3/14/2025 Posts: 10239 Rating:
|
It means the Profibus network is not correct. Take a look atWhat should you watch out for when using the RS485 repeater in PROFIBUS and MPI bus systems?There are mentioned the basic rules. Then in most of cables the wires are red and green. Green wire is connected to A and red to B. Check the wires from the starting point. Specially the intermediate devices - which cble is connected as input and which is output in Profibus connector. The final point is the position of resistor of Profibus connector. In case there is only input cable in connector the resistor is ON, If we have input and output resistor is OFF... Best regards, Hristo Mihalev
|
This contribution was helpful to
1 thankful Users |
Follow us on