5/15/2014 11:01 PM | |
Posts: 5225 Rating: (1185) |
Whomever decides to weight in on this.. Messages that are open are.. V16.3 V18.4 V18.3 V18.2 Careful that V16.3 is empty, but is referenced with a ranged bit reset. The others should be fine. Muds, I would be very careful in publishing such a program in public. My suggestion is to have a password on the ZIP file and private message Marcjan the password. Please see the x2 JPGs inside the attached ZIP file. This will give you a clue to how to do it yourself. Follow the NEXT buttons until you reach the information section. Page through the pages until you reach the empty pages (52 -54). If you energise the "message enable bit" written with the message, the message will appear. In my case............... I6.5 V18.4 ---| |----------( ) Does this help you? w Attachmentvisual clues.zip (311 Downloads) |
5/18/2014 9:48 PM | |
Posts: 12 Rating: (0) |
thanks william and marcjan for your support and confidence,,! i have done it,,it realy works fine,,!
|
This contribution was helpful to2 thankful Users |
5/21/2014 1:53 PM | |
Posts: 12 Rating: (0) |
hi,, i have uploadded screen shots,, please look into it,,n help me to solve this problem,,! and one thing more can i add new input i6.5 in machine mode sub routime to stop process of machine,,!
AttachmentNew Folder (3).zip (174 Downloads) |
5/21/2014 2:55 PM | |
Posts: 5225 Rating: (1185) |
Muds - my suggestion before was to password protect the full project files (*.mwp). I am sure the screen captures are not at risk. I will not be able to attend right now. But I publish your files here without password. @others: Please see if you guys can be of help to our fellow member. Thanks. Greetings. w AttachmentNew Folder (3).zip (185 Downloads) |
5/21/2014 8:42 PM | |
Posts: 12 Rating: (0) |
hi to all dear marcjan,,did u mean that i have to add input in main subroutinne ?
|
Follow us on