4/22/2010 1:49 PM | |
Posts: 49 Rating: (4) |
Hello I'want to connect CP cart (Simatic S5 - 6GK1143-0TB01) with PC (WinCC 7.0) On SIMATIC NET Twisted-Pair and Fiber-Optic Networks in pages 4-31 (89s) is how to pinning of the TP XP Cord 15/RJ-45. But i'm a little confused because there is two white connection. I'm using Simens simatic net industral ethernet FC TP standard cable (6XV 1840 2AH10) and ther is only white, yellow, blue and red wiring. Can i used it to pinning AUI to RJ-45 ? if yes how to do it ? Splitted from CentreCom AT210TS Adapter (AUI to RJ45). |
Last edited by: O_Moderator at: 4/22/2010 2:02 PMnew subject after splitting |
|
4/23/2010 9:27 AM | |
Posts: 49 Rating: (4) |
Thanks, for reply I have made this cable, but I still have a problem with connection. In “Network Connections” I have status “Connected” but I don’t Received and Sent any packets. I tried to scan for MAC address (SIMATIC Menager PLC => Edit Ethernet Nod …=> Browse..) but doesn’t find anything. Configuration for CPU and CP I have from this topic
“Connecting to S5 via s5 ethernet layer 4 and CP1430TF!“new.zipOne more things. If I tried this cable to connect CP 443-1 (S7400) its have different behaviors. In Network Connections I have status “Network cable unplugged” and on 2 s “Connected” and again Network cable unplugged. (CP have green “Link”, “FDX”, and “RDX” is pulsing. Cable connection configuration is only for S5 AUI ? |
4/24/2010 2:58 PM | |
Posts: 49 Rating: (4) |
|
4/24/2010 3:00 PM | |
Posts: 49 Rating: (4) |
and i used this RJ45 |
Follow us on