2/27/2018 4:27 PM | |
Joined: 5/29/2013 Last visit: 4/19/2024 Posts: 100 Rating: (28) |
What do you mean with multi IO study? https://mall.industry.siemens.com/mall/nl/nl/Catalog/Products/10046659?tree=CatalogTree Beside local IO you could extend your IO’sby using remote IO ET200SP modules. They could be connected to the Profinet interface that is already available on your CPU. If it’s for trainees to work with the PLC, than I would not advise third-party Remote i/o as you will lose some Diagnostic features, integration is a little harder (GSDML not in the TIA library), and you always need multiple support departments to get it working. |
Regards |
|
This contribution was helpful to1 thankful Users |
3/1/2018 11:55 AM | |
Joined: 5/29/2013 Last visit: 4/19/2024 Posts: 100 Rating: (28) |
Are you assuming that the i/o you have now on youCPU1212 and SM1223, is only capable of controlling LED’s ? Than you completely wrong. If my answer is not aiming to what you are trying to achieve than please specify your question or project more detailed, use even photo’s to explain more clearly. |
Regards |
|
Follow us on