12/28/2021 7:35 AM | |
Joined: 6/7/2019 Last visit: 6/9/2023 Posts: 8 Rating:
|
Hi all. I have another questions. 1) About identification of motor parameters in a stationary mode (Stationary measurement). Do I have to do it without load on the motor? Does it matter? The motor work as of lifting and lowering loads. When the parking brake is released during identification, the engine is under load.(weight of grips and other units is about 100-150 kilograms) [snip] I also wanted to write - that I am a beginner.in work with frequency converters ...Тhank you for your responses! ------------------------------------------------------------------------------------------ |
Last edited by: Alex A223 at: 12/28/2021 09:43:15Last edited by: Jen_Moderator at: 12/28/2021 09:53:42New subject after splitting. Division of question into separate topics. |
|
Follow us on