5/6/2010 11:15 PM | |
Posts: 4 Rating: (0) |
You can use also use one of the following solutions: 1)The WinCC IEC 61850 Communication Channel. You have tree license opitions: for 20, 50 or 256 devices. For more technical and order information please contactCompetence Center at Karlsruhe/DE 2)The IEC 61850 library for S7-400 (if there is a PLC in the middle). For more information: http://www.industrysolutions.siemens.com/industrial-services/it/en/products/simatic_add_ons/s7_iec61850.htm I hope it helps, |
Last edited by: O_Moderator at: 5/7/2010 12:05 PM |
|
1/26/2011 4:24 AM | |
Joined: 5/12/2010 Last visit: 1/13/2015 Posts: 1 Rating: (0) |
Hello,Mike J,I come from china,I havegot WinCC IEC 61850 Channel driver sofware,Now I want to test it,but this driver channel can act as IEC61850 MMS Client,So do you have IEC61850 MMS Server PC software?Nomatter it is siemens or third software,I hear sombody say IEC browsercan use,But italso can act as IEC61850 MMS Client
AttachmentWinCC IEC61850 Documentation_general.pdf (945 Downloads) |
9/28/2015 4:18 PM | |
Joined: 12/5/2005 Last visit: 9/25/2024 Posts: 239 Rating: (9) |
Hello,
You can contact the colleagues in charge of IEC61850 for WinCC and S7 using the e-mail function.blocks.industry@siemens.com.
Best Regards,
Márcio Santos |
Márcio Santos |
|
Follow us on