7/10/2008 12:53 PM | |
Posts: 5822 Rating:
|
Hello, you will have to choose SICAM eRTUs for this. Check the Link to get more information about these units. Best regards J_Bell |
7/10/2008 1:30 PM | |
Joined: 7/10/2008 Last visit: 11/8/2023 Posts: 32 Rating:
|
thanx I will see if there is something for us greetings pietr |
7/30/2008 9:43 AM | |
Posts: 13 Rating:
|
Hello, alternatively may you can use thevicos-rtu as an gateway (converter) betweenyour S7-400 PLC and the control-center. For example: communicationamong each other could be possible between cp343-1 inside vicos-rtu and the CP443-1 in your S7-400 PLC. Communication to the control-center(s) via IEC60870-5-104 protocol are processed with the integrated LAN-Interfaceof thevicos-rtu. |
7/31/2008 12:09 AM | |
Posts: 5 Rating:
|
Hi, beside the solutions SICAM eRTUs & vicos-rtu there exists one more possibility to "get married" between S7-World & IEC60870-5-104 (-101) protocol... Check this out: SIPLUS-RIC, Application IEC on S7 !!: maybe not applicably with S7-414H...??? |
7/31/2008 12:29 AM | |
Posts: 5 Rating:
|
|
Last edited by: s7-user at: 8/8/2008 11:27 PMLast edited by: s7-user at: 8/8/2008 1:03 AM |
|
8/3/2008 10:20 PM | |
Posts: 5 Rating:
|
Hi, a spanish company < SICA > has additional (smart...) solution for this issue. They combine S7-OPC-Server with OPC-Client/IEC60870-5-104 Gateway. Check the link. http://www.sica.es/esp/gateway.htm Regards S7-User |
11/17/2008 11:22 PM | |
Joined: 11/16/2008 Last visit: 12/12/2022 Posts: 4 Rating:
|
Hello, if not too late, please check this solution: SIPLUS RIC (Application) IEConS7: IEConS7 are differentlibraries for S7-300 and S7-400 PLCs (CPUs)for realizing telecontrol solutions with IEC 60870-5-101and 60870-5-104 (sometimes only T101 or T104) protocol. forfurther information please follow the link: https://www.automation.siemens.com/siplus/html_76/produkte/ric/softwarebibliothek.htm or contact me (GSucher ) or one of the named persons of this link: https://www.automation.siemens.com/siplus/html_76/support/service.htm PS: The latest version of IEConS7 isalso availabe forH-Systems. |
Follow us on