11/28/2017 11:46 AM | |
Joined: 9/4/2012 Last visit: 4/2/2025 Posts: 18 Rating:
|
The same problem. Another issue is that if call SaveDataRecord function via the tag which is changed in the PLC - I get system message that the record was successfully saved, but it is actaually not. Seems like a bug. If I use the same function with 'hmiOverwriteWithConfirmation' then the datarecord is saved OK. ??? BR ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/29/2017 10:45:48 AMNew subject after splitting |
|
11/29/2017 11:11 AM | |
Joined: 12/28/2015 Last visit: 2/7/2025 Posts: 256 Rating:
|
Hello therefore you should write an service request to the technical support. |
Follow us on