5/11/2019 2:22 PM | |
Joined: 2/6/2009 Last visit: 4/26/2024 Posts: 46 Rating: (23) |
Hello, I know that this tread is old, but, I run on the similar problem today. System is PCS7 V8.2 with two redundant OS Single stations - After download some changes, only on one OS station, user logon pop-up window was not opening. After initial log on, user was unable to log out, or to log-in another user. This was a problem because default user was silent log on at startup with minimum rights, not able to exit to windows or to use windows key, etc. On second OS station, everything was normal. After some testing, it looked as system was behaving as the script PASSLOGIN() was not executing at all. After performing "Regenerate Headers" in C-editor->options menu on that OS station, everything was return to normal. Something went wrong with system standard functions or whatever. EDIT: after further testing it turn out that source of problem was monitor1&2 orientation - Everything is normal ONLY if main monitor is on the left side and second monitor on the right. If you change monitor orientation to right as main no user logon pop-up is executed! Do anyone have idea how to overcome this monitor problem, and why is it happened? Best regards, VladD ------------------------------------------------------------------------------------------ |
Last edited by: VladD at: 05/11/2019 15:03:16Last edited by: VladD at: 05/11/2019 18:01:50Last edited by: Jen_Moderator at: 05/13/2019 13:01:36New subject after splitting |
|
5/20/2019 4:22 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hi, this is system behavior The monitors must not be exchanged by software, they must be physically connected properly. B.R. |
Grundkurs/Systemkurs WinCC V7: |
|