7/20/2017 8:39 AM | |
Posts: 3 Rating:
|
Hello everyone! I am having a hard time trying to make CB 1241 work normally. I have PLC - S7-1200 1214C DC/DC/DC and CB1241 (RS485). I have implemented a typical programm to load data from slave with MB_COMM_LOAD and MB_MASTER STEP7 native blocks. When I start the programm, I see that MB_COMM_LOAD is initialized and MB_MASTER always shows BUSY status. Also I started Modbus slave on PC with SimplyModbusSlave 8.0.6 and connected everything together as it is shown in manual. I can see requests in SimplyModbusSlave, bu they have wrong frame structure - 00 00 00 00 FB 00 87 00 00. If I change Slave address on MB_MASTER block from 6 to 2, I have this request frame on Slave - 00 00 00 00 FB EE 00. So definitely something is happening but I can't understand why don't I have normal frame structure? Any advice or help will be appreciated! ------------------------------------------------------------------------------------------ AttachmentModbus(RTU).zip (98 Downloads) |
Last edited by: Ondrushko at: 7/20/2017 10:40:11 AMLast edited by: Jen_Moderator at: 7/21/2017 1:12:30 PMNew subject after splitting |
|
Follow us on